{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to replace an IFM TRV00210/STRV00210 by an IFM LV434000?
The IFM was updated with several improvements and changes in the design. The firmware in both units is backwards compatible with existing installations.  In addition, the new module, LV434000, is future ready as it is designed to work with the Masterpact MTZ. See detailed differences in FAQ FA321260.

Mainly impact for substitution is the Modbus connector (5-pin connector on TRV00210/STRV00210 and RJ45 for new reference LV434000)

You can then use the following accessories to operate substitution:
  • VW3A8306D30: Cables: Rj45-open
  • VW3A8306TF03 or VW3A8306TF10: T connector 3 or 10 meters
  • VW3A8306RC: Modbus line Terminator

See examples for the following cases:
<3m>3m
CentralizedWith IFEUse Case B1Use Case B4
Without IFEUse Case B2Use Case B5
DistributedUse Case B3Use Case B6

Schneider Electric Egypt and North East Africa

Attachment(s)
New IFM use case B1-B2.png [79.75 KB]
New IFM use case B3.png [85.23 KB]
New IFM use case B4-B5-B6.png [89.87 KB]
How to replace an IFM TRV00210/STRV00210 by an IFM LV434000?
The IFM was updated with several improvements and changes in the design. The firmware in both units is backwards compatible with existing installations.  In addition, the new module, LV434000, is future ready as it is designed to work with the Masterpact MTZ. See detailed differences in FAQ FA321260.
 
Mainly impact for substitution is the Modbus connector (5-pin connector on TRV00210/STRV00210 and RJ45 for new reference LV434000)
 
You can then use the following accessories to operate substitution:
  • VW3A8306D30: Cables: Rj45-open
  • VW3A8306TF03 or VW3A8306TF10: T connector 3 or 10 meters
  • VW3A8306RC: Modbus line Terminator
 
See examples for the following cases:
 
  <3m>3m
CentralizedWith IFEUse Case B1Use Case B4
 Without IFEUse Case B2Use Case B5
Distributed Use Case B3Use Case B6

 

Schneider Electric Egypt and North East Africa

Attachment(s)
New IFM use case B1-B2.png [79.75 KB]
New IFM use case B3.png [85.23 KB]
New IFM use case B4-B5-B6.png [89.87 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.