Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to enable the Front USB port on a HMIDT732 when connected to a HMIG3U ?

The Smart Display units on the HMIGTU Series  for example  -  HMIDT732  are equipped with front USB ports.  In order to use the front USB ports,
this feature must be enabled in the Editor.

This port can be used to
- Vijeo Designer project download
-  Vijeo Designer Tool (Runtime Installer, Data Manager) access
-  PLC Communications

To enable the front USB ports for the Premium Box (HMIG3U):

1. In the Target's Hardware properties, define the Front USB Ports on Display properties. Set the USB Port (Host) and Mini USB Port (Device)
properties to Enabled.  Refer picture as shown.
USB Port (Host)
Select this option to enable the Front USB Type A port (host) on the display. If you disable this option, the operator will not be able to access
the system through the front USB port.
Mini USB Port (Device)
Select this option to enable the Front USB mini-B port (device) on the display. If you disable this option, the operator will not be able to access
the system through the front USB port.

Open Vijeo Designer then Target then Hardware

2. In the Target's General properties, make sure the Preserve Run-Time Data property is not selected. If the property is selected, the target settings
in build time will overwrite the target machine settings in runtime.

3. Download the project to the target machine, and start run time.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: