{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the PM8000 support BACnet protocol?

Product Line:
PM8000

Environment:
BACnet

Resolution:
The PM8000 meters do not support BACnet protocol

Please follow this link to view what protocols are supported by the PM8000: Protocols, ports and connections

Notes:

The meter’s fundamental protocol and architecture is ION. You can integrate the meter into various industry-standard networks. Data that the meter measures can be made available to other devices using Modbus, DNP 3.0 and SNMP, as well as the MV-90 translation system. You can configure the meter to import data from other devices on these networks. The meter supports the IEC 61850 protocol and COMTRADE waveform data format. The meter also supports IPv6, DPWS and RSTP Ethernet protocols.

Schneider Electric Egypt and North East Africa