Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the NetBotz smoke sensor NBES0307 sensitivity?
Issue:
What is the NetBotz smoke sensor sensitivity?
Product Line:
NetBotz sensors
Environment:
NetBotz smoke sensor NBES0307
Cause:
Customer request for sensor sensitivity.
Resolution:
The nominal detection sensitivity for the NBES0307 is 2.5 percent-obscuration-per-foot. This is not configurable on the sensor and the NetBotz appliance will only see the sensor as a state sensor...smoke or no smoke. A variable threshold (such as those available for a numeric sensor such as temperature) is not possible.
Please see the attached datasheet for more smoke sensor information. Please see the NetBotz product page for more recent documentation.
What is the NetBotz smoke sensor sensitivity?
Product Line:
NetBotz sensors
Environment:
NetBotz smoke sensor NBES0307
Cause:
Customer request for sensor sensitivity.
Resolution:
The nominal detection sensitivity for the NBES0307 is 2.5 percent-obscuration-per-foot. This is not configurable on the sensor and the NetBotz appliance will only see the sensor as a state sensor...smoke or no smoke. A variable threshold (such as those available for a numeric sensor such as temperature) is not possible.
Please see the attached datasheet for more smoke sensor information. Please see the NetBotz product page for more recent documentation.
Released for:Schneider Electric Egypt and North East Africa
Attachment(s)
Explore more
Range:
Explore more
Range: