Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What are the temperature rise limits for different insulation classes of dry type transformers?
The temperature rise of each winding of the transformer, designed for operation under normal service conditions, shall not exceed the corresponding limit specified in following table when tested in accordance IEC 60076-11.
The maximum temperature occurring in any part of the winding insulation system is called the hot-spot temperature.
The hot spot temperature shall not exceed the rated value of the hot-spot winding temperature specified in IEC 60076-11.


Note: When the transformer is installed inside a prefabricated substation the IEC 62271-202 standard is applicable, and the temperature rise class of the enclosure is defined,
introducing requirements on the temperature behavior of the substation (checked through a dedicated temperature rise test).

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more