Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What is the Max Torque Angle for 32R protection for a MiCOM P343
Issue
Need the to know if the MiCOM P343 can be used in the application one has. 

Product Line
MiCOM P343

Environment
Relay Protection Settings

Resolution
There is no Max Torque Angle for the 32R power protection. The element measures the 3 phase power based on the equation stated in the operation chapter in the P343 manual so there is no setting for the Max Torque Angle. The directional criteria for the power flow is either forward or reverse.

You can download the P343 manual here.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.