Issue
Need to be able to check voltage from another source using the Sepam relay.
Product Line
Sepam 20
Sepam 40
Sepam 80
Environment
Digital relays
Resolution
The MCS025 Sync-Check module only works for the Sepam 80 Series. It is not compatible with the Sepam 40 or 20 series. For more information on the MCS025 module, please refer to FA221262.
Need to be able to check voltage from another source using the Sepam relay.
Product Line
Sepam 20
Sepam 40
Sepam 80
Environment
Digital relays
Resolution
The MCS025 Sync-Check module only works for the Sepam 80 Series. It is not compatible with the Sepam 40 or 20 series. For more information on the MCS025 module, please refer to FA221262.
Released for: Schneider Electric Egypt and North East Africa