Issue:
What is the minimum firmware version of the ATV600 drive that is needed to use the VW3A3725 Bacnet card.
Product Line:
ATV600 series drives.
Environment:
All models, All serial numbers.
Cause:
Drive firmware must be of a certain level to properly operate the VW3A3725 Bacnet card.
Resolution:
A minimum firmware version of V1.8 on the ATV600 series drive is required in order to operate the VW3A3725 Bacnet MS/TP card.
What is the minimum firmware version of the ATV600 drive that is needed to use the VW3A3725 Bacnet card.
Product Line:
ATV600 series drives.
Environment:
All models, All serial numbers.
Cause:
Drive firmware must be of a certain level to properly operate the VW3A3725 Bacnet card.
Resolution:
A minimum firmware version of V1.8 on the ATV600 series drive is required in order to operate the VW3A3725 Bacnet MS/TP card.
Released for: Schneider Electric Egypt and North East Africa