{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why does the Altistart ATS22 stops everytime the start button is released?
Issue:
ATS22 stops when the start button is released

Product Line:
MCC

Environment:
8639 22U

Cause:
ATS22  stops when the start button is released

Resolution:
Verify 2 wire / 3 wire control  wiring configuration is correctly wired to the soft start.
Verify control circuit has no loose or open connections.
Verify RCR relay connections and operation.
Verify the latching circuit in the control wiring is being maintained to hold the run command.

Schneider Electric Egypt and North East Africa