{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Sepam 10 - Modbus remote indication bits for Protection Trips. Will these bits remain latched in the TRUE (or high) state until the Sepam 10 is reset following a trip?
For the Sepam 10 relay, as shown in the attached image, Remote Indication bits are provided that indicate when a trip occurs.  These Remote Indication bits can be read using Modbus communication.

However, it is important to note that these Remote Indication bits are not latched.  In other words, after the Sepam 10 sends a trip order to the circuit breaker and once the fault has been cleared, these remote indication bits will reset back to zero.

Even if the trip relay output on the Sepam 10 relay is set to Latching Mode, the Modbus Remote Indication bit will not remain latched.

In order to be sure to capture all the events from the Sepam 10, especially Protection Trips, it is essential to modify your SCADA device driver to read the time-tagged events from the Sepam relay.  Using the Remote Indication bits is not reliable, and you run the risk of missing events if a fault occurs during a communications outage.

AEDL3

Schneider Electric Egypt and North East Africa

Attachment(s)
KB_2017_Sepam10_Modbus_RemoteIndications_Not_Latched.jpg [207.85 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.