{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

PME/PSO: SQL Server Licensing Details

Issue
SQL Server licensing overview for Power Monitoring Expert and PowerSCADA Operation (Advanced Reporting and Dashboards Module).

Product Line
PowerSCADA Operation 8.x
Power Monitoring Expert 8.x

Environment
PowerSCADA Operation (Advanced Reporting and Dashboards Module)
Power Monitoring Expert
SQL Server

Resolution
PME 8.x Standard, PME 8.x DC, and PME 8.x HC, and PowerSCADA Advanced Reporting support SQL Server 2012, 2014 and 2016.

SQL Server 2016 pricing has significantly increased from Microsoft, so we continue to provide/ship SQL Server 2012 from the factory.

  • SQL Server 2012 will be available to us until April 2018
  • Product supports SQL Server 2016, SQL Server 2014, SQL Server 2012 and 2008R2
The Per-Core licence (recommended)
  • Allows unlimited users and devices to access the database.
  • Requires one licence for each Core on the server where SQL is installed.
  • Being 4 the minimum number of cores sold (in the case of single core and dual core processors)
The SERVER/CAL licence (not recommended)
  • Requires one CAL for each user and device. (A device includes any meter that has its data logged in the PME database, even via PC logging)
  • Requires a SERVER licence for every machine where a component of SQL is installed.
  • More complicated and expensive for systems with ~30 meters + users.
  • Cannot be upgraded to a Processor licence.

Schneider Electric does not promote or provide (SERVER/CAL) licensing option from the factory for these reasons.

The part numbers for SQL Server Standard Edition licenses are PSWSQL2012L or PSWSQL2016L

The MINIMUM licensing is always 4 Cores:

2x PSWSQL2012L
OR
2x PSWSQL2016L

SQL Server Standard Edition is licensed per core:
Number of core licenses required = Total cores on the server
Licence sold in 2-core packs

Example: 2 Intel Xeon 6-core processors
Number of core licenses required = 12 (total cores on the server)
Purchase 6 licenses (licence sold in 2-core packs)

Schneider Electric Egypt and North East Africa

Attachment(s)

[PME] Power Management Systems - Licensing Overview.pptx[PME] Power Management Systems - Licensing Overview.pptx [924.51 KB]
Explore more
Range:
EcoStruxure™ Power SCADA Operation 8.2EcoStruxure™ Power Monitoring Expert 8.2
Explore more
Range:
EcoStruxure™ Power SCADA Operation 8.2EcoStruxure™ Power Monitoring Expert 8.2
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.