{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PLC application is lost on the TSXP57204 after running for 48-72 hours following addition of memory card.
Issue
PLC application is lost on the TSXP57204 after running for 48-72 hours following addition of memory card.

Product Line
Unity, TSXP57204

Environment   
Windows 10


Resolution
 
After 48-72 hours following the adding of a memory card to Premium Unity application that has been running fine for awhile, the
PLC loses the application.  The PLC is still powered up.

The reason this could occur may be due to a mechanical problem with the PCMCIA memroy card slot or something internal to the 
PCMCIA connector.  

If this occurs, it is recommended to replace the PLC.

 

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top