Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is meant by vector group for transformers and why is it important?

What is vector group for transformers?
A vector group is the International Electrotechnical Commission (IEC) method of categorizing the high voltage (HV) windings and low voltage (LV) winding configurations of three-phase transformers.
The vector group designation indicates the windings configurations and the difference in phase angle between them.
Example: a wye HV winding and delta LV winding with a 30-degree lead is denoted as "Yd11".

Common vector group presentations are tabulated below. 
image 1 

Why is the vector group important to specify? 

As different combinations of winding connections will result in different phase angles between the voltages on the windings, transformers connected in parallel must have the same vector group because the mismatching of phase angles will result in circulating current and other system disturbances.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: