Search FAQs
RTC Synchronization with Time Zone over Internet in M172 performance controller
M17xP supports this BIBBS (Bacnet interoperability building blocks):
DM-TS-B(*) TimeSynchronization-B
so a Bacnet supervisor can synchronize it.
NTP (Network time protocol) is most common and widely used network protocol among the protocols used for clock synchronization of device over network
Today NTP / SNTP is not supported on M17xP controllers so it is not possible to synchronize the RTC of it to the NTP server.
DM-TS-B(*) TimeSynchronization-B
so a Bacnet supervisor can synchronize it.
NTP (Network time protocol) is most common and widely used network protocol among the protocols used for clock synchronization of device over network
Today NTP / SNTP is not supported on M17xP controllers so it is not possible to synchronize the RTC of it to the NTP server.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: