This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
Issue: The installation guide for for the APC Din Rail/Panel Mount UPS Battery Replacement specifies how to connect an External Battery to the UPS.
Product Range: SUA500PDR-S, SUA500PDR-H
Resolution:
These UPS models do not have extended run capability. The installation guide refers to the feature that allows connecting the RBC externally to the UPS. The purpose for attaching a battery externally to the UPS is to accommodate installation requirements for specific applications that require the UPS to be enclosed with control devices in an 'air tight' enclosure. Batteries should not be inside this type of enclosure. With the chassis design on SUA500PDR models, the associated battery can be mounted in a separate appropriately vented enclosure by using the extended length cable included with the battery.
Product Range: SUA500PDR-S, SUA500PDR-H
Resolution:
These UPS models do not have extended run capability. The installation guide refers to the feature that allows connecting the RBC externally to the UPS. The purpose for attaching a battery externally to the UPS is to accommodate installation requirements for specific applications that require the UPS to be enclosed with control devices in an 'air tight' enclosure. Batteries should not be inside this type of enclosure. With the chassis design on SUA500PDR models, the associated battery can be mounted in a separate appropriately vented enclosure by using the extended length cable included with the battery.