{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What to do when the "Write to device" operation fails with Ecoreach when connected to Micrologic X along with Enerlin'X IO Module?
The "Write to device" operation fails with Ecoreach when connected to Micrologic X along with Enerlin'X IO module. In this case, the Cradle management application is selected on the IO module i.e. the IO module rotary switch is set to position 2. When with Ecoreach "Write to device" operation fails, an appropriate error message "Unable to write to project due to spelling mismatch for Cradle event. Please do a write to the device and try again" is displayed in Ecoreach Error window.As described in the Error message the "Write to operation" failed due to the discrepancy in the spelling of "Cradle" between Ecoreach and the Enerlin'X IO module.

Workaround: To solve this issue, it is suggested to do the "Write to device" operation first as suggested in the Ecoreach Error Message and wait for 30 seconds.

After following as suggested in the Workaround the subsequent "Write to device" operation(s) from Ecoreach will be successful.

Schneider Electric Egypt and North East Africa