{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the BACnet option cards VW3A3725 available on the ATV630 Process Drives?
Issue:
ATV630 Process Drives Bacnet option cards availability.

Product Line:
Altivar ATV630 only

Resolution:
The BACnet part number is VW3A3725, is a BACnet MS/TP module for ATV600 series drives. They are not compatible with ATV900 series drives.
Note that the ATV630, ATV650, ATV680, and ATV660 drive Firmware needs to be minimum V1.8.

Schneider Electric Egypt and North East Africa

Attachment(s)
Bacnet MS TP VW3A3725.pdf [2.09 MB]