Search FAQs
What would cause a EPF2 fault using Profinet's telegram 1 and I/O profile on the ATV630 and ATV930 drives?
Issue:
EPF2 fault causes using Profinet and I/O profile on the ATV630 and ATV930 drives.
Product Line:
ATV630, ATV930
Environment:
All
Cause:
IO Profile and Telegram 1 are not compatible.
Resolution:
Profinet telegram 1 is not supported with IO Profile. It is suggested that they use telegram 100 which does support IO Profile.
EPF2 fault causes using Profinet and I/O profile on the ATV630 and ATV930 drives.
Product Line:
ATV630, ATV930
Environment:
All
Cause:
IO Profile and Telegram 1 are not compatible.
Resolution:
Profinet telegram 1 is not supported with IO Profile. It is suggested that they use telegram 100 which does support IO Profile.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: