{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is it possible to control Altistart ATS01N2 from PLC (transistor output) directly to LI input of ATS01N2?

Direct connection of PLC 24V transistor output to LI1 or LI2 on Altistart ATS01 is not possible. If your PLC does not have relay output, use interposing reply (coil voltage e.g 24V). Then connect relay contact to LI+ and LI2 for the On /OFF command for ATS01.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Altistart 01
Explore more
Range:
Altistart 01
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.