{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PME 8.2 WebReach displays an 'X' object for grouping objects which are set to the transparent option
Issue
A customer is seeing 'X''s on grouping objects which are set to the transparent option when viewed through the Diagrams section of Web Applications as seen below.  This same issue does not occur within Vista.



Product Line
PME 8.x
PME 7.x

Environment
Web Applications - Diagrams

Cause
File permissions are not set correctly on the directory where PME is installed.

Resolution
The virtual roots inside web applications can be configured for either Anonymous Authentication or a specific Windows account.  This account needs to have full read/write permissions over the PME installation folder as well as the image file "transparent.jpg" within the C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\config\diagrams\images\Status_Graphics directory.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.