{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the purpose of Relay in PM1130H meter ?
Relay is used to trigger an alarm or a secondary system based on a preset condition in the meter.

The relay is Normally Open (NO) when not triggered. When triggered (operated) it changes to Normally Closed (NC).

A relay can be triggered depending on source of operation. The supplied source can be utility, alternate source, or both.

Schneider Electric Egypt and North East Africa