{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
This FAQ has been written for NEAL (North East Africa and Levant) region. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
What is the maximum THDI% permissible for Micrologic 6.0A trip unit equipped with NW12H2-3P-FIXED-85KA?
Thanks to be informed that ,
there is no permissible THD limit for a circuit breaker. The THDi and THDv for networks are generally guided by IEEE 519-2014 and IEC 61000-4-7 standards.

2. Micrologic A trip units do not offer measurements or protections in case of harmonics. In case harmonic measurements and indicators were required, you will have to opt-to Micrologic H. Micrologic H is the only Micrologic trip unit with harmonics measurements capability.

3. Harmonics will generally cause nuisance tripping to all circuit breakers. Thus, when having a harmonics generator in your network, you are advised to use a choke or line reactor to remove/mitigate the harmonics. You can also use passive or active filters in some cases. "

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: