Issue:
How can you set up the ATV21 or ATV212 drive to follow a 0 - 5Vdc speed reference signal?
Product Line:
Altivar ATV21, ATV212 and S-flex drive
Environment:
All
Cause:
Speed reference input on VIB to be 0 - 5Vdc, not the default 0 - 10Vdc
Resolution:
The VIB analog input is scaled with parameters F210 thru F213, based on a rated 10Vdc maximum input. Assign reference points as follows:
Reference point 1
F210 = 0% (of the 10Vdc max, 0Vdc)
F211 = 0Hz
Reference point 2
F212 = 50% (of the 10Vdc max, 5Vdc)
F213 = 60Hz
On the ATV212 drive, set DIP switch SW100 for VIB to the left (U).
Set FMOd = 2
How can you set up the ATV21 or ATV212 drive to follow a 0 - 5Vdc speed reference signal?
Product Line:
Altivar ATV21, ATV212 and S-flex drive
Environment:
All
Cause:
Speed reference input on VIB to be 0 - 5Vdc, not the default 0 - 10Vdc
Resolution:
The VIB analog input is scaled with parameters F210 thru F213, based on a rated 10Vdc maximum input. Assign reference points as follows:
Reference point 1
F210 = 0% (of the 10Vdc max, 0Vdc)
F211 = 0Hz
Reference point 2
F212 = 50% (of the 10Vdc max, 5Vdc)
F213 = 60Hz
On the ATV212 drive, set DIP switch SW100 for VIB to the left (U).
Set FMOd = 2
Released for:Schneider Electric Egypt and North East Africa