{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why can I not see Display Configuration Menu on ATV61 drives?
Issue:
Display Config under the Main Menu is not visible.

Product line:
Altivar 61, ATV61

Environment:
n/a

Cause:
n/a

Resolution:
To see the Display Config menu, the drive must be in Access Level of Advanced or Expert. You also have to have the Password function deactivated or turned off.

Schneider Electric Egypt and North East Africa