Search FAQs
Is the VW3A1111 keypad compatible for use with the ATV320 drives?
Issue:
Will the VW3A1111 keypad work with the ATV320 drives?
Product Line:
ATV320
Environment:
All serial numbers
Cause:
Installation
Resolution:
Both the ATV320 VFD and the VW3A1111 keypad firmwares have been upgraded to support compatibility. (6-2019)
Firmware versions required:
ATV320 V2.9IE37#3
VW3A1111 V2.0IE53
Earlier versions are not compatible.
VW3A1111 is supported for use with the ATV6x0, ATV9x0 and ATV340 VFD product lines.
The ATV320 is also compatible with keypads VW3A1101, VW3A1006 and VW3A1007.
Note: Early versions of the ATV320 catalog included the VW3A1111 keypad by mistake, but was removed from the Sept 2018 catalog.
Will the VW3A1111 keypad work with the ATV320 drives?
Product Line:
ATV320
Environment:
All serial numbers
Cause:
Installation
Resolution:
Both the ATV320 VFD and the VW3A1111 keypad firmwares have been upgraded to support compatibility. (6-2019)
Firmware versions required:
ATV320 V2.9IE37#3
VW3A1111 V2.0IE53
Earlier versions are not compatible.
VW3A1111 is supported for use with the ATV6x0, ATV9x0 and ATV340 VFD product lines.
The ATV320 is also compatible with keypads VW3A1101, VW3A1006 and VW3A1007.
Note: Early versions of the ATV320 catalog included the VW3A1111 keypad by mistake, but was removed from the Sept 2018 catalog.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: