Search FAQs
What are the specs for the fiber optic communication in the ION 8650 meter
Issue
Want to know the specification of fiber optic communication with the ION8650 meter
Product Line
ION8650
Environment
Fiber optic communication
Resolution
The part used for fiber optic communication is AFBR-5803AQZ from Broadcom Link to site.
Want to know the specification of fiber optic communication with the ION8650 meter
Product Line
ION8650
Environment
Fiber optic communication
Resolution
The part used for fiber optic communication is AFBR-5803AQZ from Broadcom Link to site.
Connector Type | SC |
Data Rate | 125 MBd |
Emitter | LED |
Fiber Type | Multimode Glass |
Maximum Distance (m) | 2000 |
Nominal Optical Wavelength (nm) | 1300 |
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: