{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Network discovery returns the error 'Chassis ID conflict.
Issue
Network discovery returns the error 'Chassis ID conflict.

Product Line
Connexium Network Manager

Environment
Windows 10


Resolution
After discovering the network, Connexium Network manager returns the error 'Chassis ID conflict'
fggg



The error message indicates that both devices (i.e., 192.168.11.3 and 192.168.11.4) have the same LLDP chassis ID.
The reason for the error is because LLDP (Link Layer Discovery Protocol) requires the chassis ID to be unique. The chassis ID is based on the system name.


To resolve the error, check the system name for both devices and verify that they are unique using the following steps.
  • Open the 'device' list by clicking on the 'Device' tab.
  • Verify that the names are unique.
gfgg




If the 'system Name' is not unique, use the following steps to change it.
  • Open the network topology map by clicking on the 'Map'.
  • Right click on the device icon.
  • Select 'Properties'.
gg

  • Chnge the name.
  • Click on OK.
gfg

Schneider Electric Egypt and North East Africa