Search FAQs
How can I add a Profibus GSD file to Unity Pro library of Generic DTMs?
Issue
How can I add a Profibus GSD file to Unity Pro library of Generic DTMs?
Product Line
EcoStruxure Control Expert, M580, M340, Quantum
Environment
BMEP581020 v2.70, TCSEGPA23F14F, Unity Pro v13.0.
Resolution
The TCSEGPA23F14F (PRM) is a standalone module designed to provide Profibus DPV0 & DPV1 master capability to the M340, M580, Premium and Quantum ranges. Profibus slave configuration is based on GSD that is a data base file with the device information and I/O configuration that is provided by the vendor's.
The PRM Master DTM and the PRM Gateway DTM includes an interface for converting any GSD file into a generic DTM in order to be integrated into the DTM catalog and used to configure a Profibus slave for the PRM.
P.S.: You can download here the PROFIBUS Remote Master iso file that includes the PRM Master DTM and PRM Gateway DTM.
How can I add a Profibus GSD file to Unity Pro library of Generic DTMs?
Product Line
EcoStruxure Control Expert, M580, M340, Quantum
Environment
BMEP581020 v2.70, TCSEGPA23F14F, Unity Pro v13.0.
Resolution
The TCSEGPA23F14F (PRM) is a standalone module designed to provide Profibus DPV0 & DPV1 master capability to the M340, M580, Premium and Quantum ranges. Profibus slave configuration is based on GSD that is a data base file with the device information and I/O configuration that is provided by the vendor's.
The PRM Master DTM and the PRM Gateway DTM includes an interface for converting any GSD file into a generic DTM in order to be integrated into the DTM catalog and used to configure a Profibus slave for the PRM.
- In the Unity Pro menu bar, select Tools -> DTM Browser
- In the DTM Browser, select the PRM_Master instance or PRM_Gateway instance as applicable
- Right click (DTM contextual menu) and select Device menu -> Add GSD in Library. The welcome page of the wizard opens.
- Click Next, select the location of the GSD File of the Profibus slave that you want to add and go forward until a page with finish option opens. (E.g., the GSD provided by Pepperl+Fuchs for the PROFIBUS Gateway DP/PA HD2-GTR-4PA)
- Unity Pro hardware catalog has to be updated in order to use new devices with your Unity Pro project.
- Select in the Unity Pro menu bar, Tool->Hardware Catalog
- Select DTM Catalog tab in the Hardware catalog windows
- Click the Update button for starting the update
P.S.: You can download here the PROFIBUS Remote Master iso file that includes the PRM Master DTM and PRM Gateway DTM.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: