{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you wire and program an ATV630 to replace an ATV58 in a Trane Air Handler?
Issue:
Wondering how do you program an ATV630, to replace an ATV58, in a Trane Air Handler

Product Line:
ATV630

Environment:
All

Cause:
Wiring and programming

Resolution:
A Trane Unit had a board that did the switching for the drive.  If you've wired exactly as before, you only need to Program [Complete settings] > [Command and Reference] > [Ref Freq.1Cfg]  to AI1 and [Complete Settings] [Input/Output] [R2 Configuration] to Drive Running.  Be sure to configure [Simply Start].

Schneider Electric Egypt and North East Africa