{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
For what applications can we use PM1130H meter ?
PM1130H meter can be used for dual source accounting applications that involve two
energy registers, for example Utility vs Genset, Utility vs Solar, Utility vs Wind, or a
combination of any two-power source.

It can also be used in installations that require split energy monitoring for
two conditions, for example, running and idle. You can form a relay to control the
load in event of abnormalities such as excessive power consumption or electric
faults.

The meters can be used for secondary billing application in large commercial
complexes or buildings as tenant meters in custom panels, switch boards, switchgear,
Gen-set panels, non-renewable energy panels, and OEM panel boards.

Schneider Electric Egypt and North East Africa