{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Can I to create an array of structure in SoMachine V4.3 be exported to Vijeo Designer?
Yes, an array of structure created in SoMachine can be exported to Vijeo Designer.
First create a structure in SoMachine.  For an array of structure, create a regular array and select the structure name for the data type.
To export to SoMachine, right-click on the Symbol Configuration and select export to Vijeo Designer.

Schneider Electric Egypt and North East Africa