{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to choose the file extension when a SD card is used for datalogging with M580/M340?
Issue

When creating a file named ‘Test' and write the contents of %MW1-100 to test, what is the file format of 'Test' using SD card and data file? Can this file 'Test' be viewed outside of Unity? Is there a file extension associated with 'Test'?
The help files suggest that after FTP'ing into the SD card we can copy & paste the file into other applications. What applications would that be?

Product Range

M580, SD card

Resolution

When creating a file in Unity pro using SD card and file management library, if the user does not specify the file extension, the result of the created file in a FTP client will be with “no extension”



To associate a file extension, user MUST specify the type of file in Unity pro as show below; the created file can then be opened with appropriate software.

Schneider Electric Egypt and North East Africa