Issue:
Ramp increment meaning on the Altivar Process drive.
Product Line:
Altivar Process ATV600 ATV900
Environment:
All serial numbers
Cause:
N/A
Resolution:
Ramp increment is a parameter that will affect the resolution and the range of acceleration and deceleration parameters.
Inr [Ramp increment]
0.01 [0.01]: Ramp up to 99.99 seconds
0.1 [0.1]: Ramp up to 999.9 seconds
1 [1]: Ramp up to 6,000 seconds
This parameter is valid for [Acceleration] (ACC), [Deceleration] (dEC), [Acceleration 2] (AC2) and [Deceleration 2] (dE2).
Ramp increment meaning on the Altivar Process drive.
Product Line:
Altivar Process ATV600 ATV900
Environment:
All serial numbers
Cause:
N/A
Resolution:
Ramp increment is a parameter that will affect the resolution and the range of acceleration and deceleration parameters.
Inr [Ramp increment]
0.01 [0.01]: Ramp up to 99.99 seconds
0.1 [0.1]: Ramp up to 999.9 seconds
1 [1]: Ramp up to 6,000 seconds
This parameter is valid for [Acceleration] (ACC), [Deceleration] (dEC), [Acceleration 2] (AC2) and [Deceleration 2] (dE2).
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for: Schneider Electric Egypt and North East Africa