{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ATV680 does the drive show the Frequency Reference in idle state?
Issue:
Does the ATV680 show the Freq Ref in idle state?

Product:
ATV6xx ATV9xx

Environment:
All serial numbers

Cause:
ATV680 pump off  and the drive is in the rdy state.

Resolution:
Yes, the drive default will the display the frequency reference, unless otherwise modified by customer to show output frequency or motor current which would show 0.0 in idle state. If the drive is left at default to show Frequency Reference and shows 0.0, check the reference signal from the programmed source.
Possible sources could be:
  • Analog input
  • HMI (keypad)
  • Communication
  • Preset speed
  • Jog
  • PID control
  • other, depending on the programming in the drive.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: