{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Power Monitoring Expert - Insufficient SQL Server Role to open Database Manager

Issue:
The following error is displayed when trying to open the Database Manager: cannot open the Database Manager. To open the Database Manager a user must be a member of the SQL sysadmin server role.

Description of sysadmin server role error from SQL

Product Line:
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment:
Database Manager
SQL Server Management Studio (SSMS)

Cause:
The 'sysadmin' role is not applied to the user account in SQL.

Resolution:
In order to use the Database Manager in Power Monitoring Expert 8.1 and newer, the user must log into Windows using an account that has been granted 'sysadmin' role in SQL Server Management Studio.

*Warning: Irreparable Database Damage can occur.  This procedure should only be performed by users familiar with SQL Server Management Studio.  Databases should be backed up prior to performing this procedure.*
Note: In some cases, a domain account may appear to have the 'sysadmin' role checked in SQL but are still unable to log in due to domain policy restrictions. To check and see if the user account does indeed have 'sysadmin' rights, the following query can be run in SQL Server Management Studio.

SELECT IS_SRVROLEMEMBER ('sysadmin',' <domain-user')

Checking server role and where to select

If the value returned is zero '0' the user does not have sysadmin rights.

Note: More information on how to determine if a SQL Server login is a member of a specified server role can be found in FA346467 .

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: