Search FAQs
Whether ATV212 is compatible with Pasive Harmonic Filter
We cannot connect the passive filter due to C less capacitor which enter in resonance with the DC bus. There is no offer with ATV212 to reach 5% THDI.
Basically the drive is designed to reach 48% THDI, but no input filter offer is existing to decrease the THDI (neither line choke nor active filter).
The target of this product is to compliant with the standart IEC61000-3-12 so THDi above 48%. Our product achieve around 35% of THDi.
Basically the drive is designed to reach 48% THDI, but no input filter offer is existing to decrease the THDI (neither line choke nor active filter).
The target of this product is to compliant with the standart IEC61000-3-12 so THDi above 48%. Our product achieve around 35% of THDi.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: