{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the HMIG3U support Dialog Table in Vijeo Designer?
Issue:
Checking compatibility of an old project when migrating to HMIG3U. Does the HMIG3U also support the dialog table feature?

Product Line:
Magelis, HMIG3U, Vijeo Designer

Resolution:
Yes, the HMIG3U supports the dialog table feature in Vijeo Designer when the appropriate protocol is used. For example, Modbus TCP/IP.

Note that protocols that use Tag names as device addresses do not support the Dialog Table. For example, Somachine or Pac Drive Ethernet.

Schneider Electric Egypt and North East Africa