{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What causes a CFF [Configuration Fault] on an ATV320 drive?

Issue:
What are some possible causes for getting a CFF fault on an ATV320 drive?

Product Line:
Altivar 320

Environment:
All

Cause:
Configuration error

Resolution:
CFF= incorrect configuration or an option card has been removed which will require the drive to set back to factory default.

Probable Causes:
• Option card changed or removed.
• Control block replaced by a control block configured on a drive with a different rating.
• The current configuration is inconsistent.

Remedies:
• Check that there are no card errors.
• In the event of the option card being changed/removed deliberately, see the remarks below.
• Check that there are no card errors.
• In the event of the control block being changed deliberately, see the remarks below.
• Return to factory settings or retrieve the backup configuration, if it is valid


Option card changed or removed
When an option card is removed or replaced by another, the drive locks in [Incorrect config.] (CFF) fault mode on power-up. If the card has been deliberately changed or removed, the detected fault can be cleared by pressing the ENT key twice, which causes the factory settings to be restored (see page 81) for the parameter groups affected by the card. These are as follows:
Card replaced by a card of the same type
• Communication cards: only the parameters that are specific to communication cards

Control block changed
When a control block is replaced by a control block configured on a drive with a different rating, the drive locks in [Incorrect config.] (CFF) fault mode on power-up. If the control block has been deliberately changed, the detected fault can be cleared by pressing the ENT key twice, which causes all the factory settings to be restored.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Category: