Search FAQs
What is the difference between LI1 and DI1 on altivar drives?
Issue:
The difference between logic input LI1 and digital input DI1
Product Line:
Altivar Drives
Environment:
ATV12, ATV312, ATV320, ATV71, ATV61, ATV600, ATV900, ATV58, ATV66, ATV11, ATV28, ATV18, ATV16
Cause:
Manual refers to LI inputs and Drive terminal refer to Digital inputs.
Resolution:
LI1 is a programmable logic input.
DI1 is a programmable digital / logic input.
Technically, they are the same.
The difference between logic input LI1 and digital input DI1
Product Line:
Altivar Drives
Environment:
ATV12, ATV312, ATV320, ATV71, ATV61, ATV600, ATV900, ATV58, ATV66, ATV11, ATV28, ATV18, ATV16
Cause:
Manual refers to LI inputs and Drive terminal refer to Digital inputs.
Resolution:
LI1 is a programmable logic input.
DI1 is a programmable digital / logic input.
Technically, they are the same.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Category:
Explore more
Category: