Search FAQs
How can you monitor the status of the digital inputs on the ATV630 and ATV930 Process drives?
Issue:
Monitoring the status of the digital inputs on the Process drives
Product Line:
ATV630 and ATV930
Environment:
All
Cause:
Wants to monitor the status of logic input DI11
Resolution:
Address 5202 will show the status of the logic inputs. if you want to monitor DI11 its bit 11 of the 5202 address.
"IL1I
IL1R" Bit 0: Value of LI1.
Bit 1: Value of LI2.
Bit 2: Value of LI3.
Bit 3: Value of LI4.
Bit 4: Value of LI5
Bit 5: Value of LI6
Bit 6: Reserved (= 0).
Bit 7: Reserved (= 0).
Bit 8: Reserved (= 0).
Bit 9: Reserved (= 0).
Bit 10: Reserved (= 0).
* Bit 11: Value of LI11
Bit 12: Value of LI12
Bit 13: Value of LI13
Bit 14: Value of LI14
Bit 15: Value of LI15
Monitoring the status of the digital inputs on the Process drives
Product Line:
ATV630 and ATV930
Environment:
All
Cause:
Wants to monitor the status of logic input DI11
Resolution:
Address 5202 will show the status of the logic inputs. if you want to monitor DI11 its bit 11 of the 5202 address.
"IL1I
IL1R" Bit 0: Value of LI1.
Bit 1: Value of LI2.
Bit 2: Value of LI3.
Bit 3: Value of LI4.
Bit 4: Value of LI5
Bit 5: Value of LI6
Bit 6: Reserved (= 0).
Bit 7: Reserved (= 0).
Bit 8: Reserved (= 0).
Bit 9: Reserved (= 0).
Bit 10: Reserved (= 0).
* Bit 11: Value of LI11
Bit 12: Value of LI12
Bit 13: Value of LI13
Bit 14: Value of LI14
Bit 15: Value of LI15
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: