{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Maximum number of BMXNOR0200 module which can be installed with a Modicon M580 CPU local rack.

Issue:
What is the Maximum number of BMXNOR0200 module which can be installed with a Modicon M580 CPU local rack?

Product Line:
BMXNOR0200H

Environment:
All

Resolution:
The maximum number of BMXNOR0200 which can be installed within a local rack containing M580 CPU is 6.
It also depends on the model of M580 CPU is being used.

1. BMEP58 6040 can accommodate 6 BMXNOR0200 modules.
2. BMEP58 5040 can accommodate 4 BMXNOR0200 modules.
3. BMEP58 4040 can accommodate 4 BMXNOR0200 modules.
4. BMEP58 4020 can accommodate 4 BMXNOR0200 modules.
5. BMEP58 3040 can accommodate 3 BMXNOR0200 modules.
6. BMEP58 3020 can accommodate 3 BMXNOR0200 modules.
7. BMEP58 2040 can accommodate 2 BMXNOR0200 modules.
8. BMEP58 2020 can accommodate 2 BMXNOR0200 modules.
9. BMEP58 1020 can accommodate 2 BMXNOR0200 modules.

Schneider Electric Egypt and North East Africa