{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can you change the display on the ATV212 or S-flex drive to show motor speed hz vs amps?
Issue:
Show motor speed hz vs amps on the ATV212 display.

Product Line:
ATV212 or S-flex

Environment:
All

Cause:
Needs to change the display to show motor speed in hz not amps.

Resolution:

Setting Function
F710

Motor operating frequency
(Hz or custom display, see F702 on
page 83)

1 Speed reference (Hz or custom display,
see F702 on page 83)

2 Motor current (% or A, see F701)

3 Drive controller rated current (A)

4 Drive controller thermal state (%)

5 Output power (kW)

6 Internal speed reference (after PID
function) (Hz or custom display, see F702
on page 83)

7 Serial communication data

8 Output speed (rpm, see F417 on page 97)

9 Displays the total number of frames
received by the communication card since
the last power ON

10 Displays the total number of valid frames
received by the communication card since
the last power ON

Schneider Electric Egypt and North East Africa

Attachment(s)
ATV212 F710.JPG.jpg [112.34 KB]