{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How do you configure the ATV320 drive for a bipolar +10/-10vdc speed control?

Article available in these languages: Japanese, Turkish

Issue:
Configuring the ATV320 drive for a bipolar +10/-10vdc speed control?

Product Line:
ATV32 and ATV320 Drives

Environment:
All

Cause:
Wants to set up the drive so 0 to 10vdc is FWD and 0 to - 10vdc is REV

Resolution:
AI2- [AI2 CONFIGURATION]
Programming
CONF
FULL
I/O menu
AI2 configuration


AI2t [AI2 Type] [Voltage +/-] (n10U)
Set this to (n10U) for Positive and negative voltage input.
[Voltage +/-] (n10U): Positive and negative voltage input +/- 10 V (the input is bidirectional)
UIL2 [AI2 min value] 0V
AI2 voltage scaling parameter of 0%.
UIH2 [AI2 max. value] V 10.0 V
AI2 voltage scaling parameter of 100%.

Note that the Min range is 0v and max is 10 vdc this will still allow for -10 to 10vdc  with 0-10v REV and 0 +10v FWD

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: