{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the switchgear control failure codes?

  • A code appears in Event log for each control operation:
Code      Reason
0              Command completed successfully
1              Local command blocked because switch position is intermediate or unknown
2              Local command blocked because switch position is already in correct state
3              Local command canceled by user
4              Switch position did not change within configured maximum operation time
5              Command blocked by Head Unit interlocks, e.g. motor supply fault or battery low
6              Command failed due to timeout waiting for enable from Head Unit
7              Local command blocked because disabled by configuration
8              Local command blocked because local/remote status is unknown
9              Local command blocked because local/remote status is remote
10           Local command blocked because automation is on
11           Remote command blocked because automation is on
12           Sectionalizer command blocked because automation is off
13           Sectionalizer command blocked because local/remote status is unknown
14           Sectionalizer command blocked because local/remote status is local
15           Unexpected command source (firmware error)
16           Remote command blocked because requested position is not a valid value
17           Command blocked because a command is already in progress for this module
18           Command blocked because the power shutdown signal is active
19           Command blocked because a command is already in progress for another module
20           Command blocked because measured switch position is intermediate or unknown
21           Command blocked because measured switch position is the same as the requested position
22           Command blocked because earth switch position is open
23           Open command blocked because external input is false
24           Open command blocked because external input is true
25           Close command blocked because external input is false
26           Close command blocked because external input is true
27           Commands blocked because module behaviour mode is off

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.