Issue
Profibus slaves has a diagnostic message and STBNDP2212 has 32 bytes with mandatory Profibus DP diagnostic, diagnostic information about the status of the island bus and specific health data
Product Line
Advantys STB, TCSEGPA23F14F (PRM), EcoStruxure Control Expert (formerly known as Unity Pro)
Environment
TCSEGPA23F14F, Unity Pro v13.0, STBNDP2212, Advantys v11
Resolution
The TCSEGPA23F14F (PRM) is a standalone module designed to provide Profibus DPV0 & DPV1 master capability to the M340, M580, Premium and Quantum ranges. This video will show you how to read/interpret the data on Profibus DP diagnose of a STBNDP2212 and you can use it for the module diagnostic. E.g., read the health of each module of the STBNDP2212.
Profibus slaves has a diagnostic message and STBNDP2212 has 32 bytes with mandatory Profibus DP diagnostic, diagnostic information about the status of the island bus and specific health data
Product Line
Advantys STB, TCSEGPA23F14F (PRM), EcoStruxure Control Expert (formerly known as Unity Pro)
Environment
TCSEGPA23F14F, Unity Pro v13.0, STBNDP2212, Advantys v11
Resolution
The TCSEGPA23F14F (PRM) is a standalone module designed to provide Profibus DPV0 & DPV1 master capability to the M340, M580, Premium and Quantum ranges. This video will show you how to read/interpret the data on Profibus DP diagnose of a STBNDP2212 and you can use it for the module diagnostic. E.g., read the health of each module of the STBNDP2212.
Released for:Schneider Electric Egypt and North East Africa