Search FAQs
Video : How to recover information from DRS switch and modify the configuration file?
Issue
Schneider Electric provides pre-defined configuration for ConneXium DRS switches and you can verify the configuration used on your switch by the WebPage
Product Line
Modicon Switch, ConneXium Switch
Environment
TCSESM083F23F1, TCSESM083F23F1C, TCSESM063F23CU1, TCSESM063F23CU1C, TCSESM063F23CS1, TCSESM063F23CS1C.
Resolution
The extended managed ConneXium switches (part numbers listed above) are Dual Ring Switches that can be used in complex M580 or Quantum architectures to perform these functions:
Schneider Electric provides pre-defined configuration for ConneXium DRS switches and you can verify the configuration used on your switch by the WebPage
Product Line
Modicon Switch, ConneXium Switch
Environment
TCSESM083F23F1, TCSESM083F23F1C, TCSESM063F23CU1, TCSESM063F23CU1C, TCSESM063F23CS1, TCSESM063F23CS1C.
Resolution
The extended managed ConneXium switches (part numbers listed above) are Dual Ring Switches that can be used in complex M580 or Quantum architectures to perform these functions:
- Integrate fiber cable on the main ring
- Enable distributed equipment to participate on the RIO network
- Enable RSTP recovery support for devices on the sub-rings
- Isolate the sub-rings
- Provide redundancy between the main-ring and a sub-ring
- Separate primary and standby PACs in a long-haul Hot Standby system
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: