Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
How can I activate / deactivate a driver in Vijeo Designer associated to a PLC?

You can write the values 1 or 0 to turn on (1) or off (0) the communication with the associated equipment. A value of 2 indicates the driver is offline for this specific equipment.

When State is 0, communication with the associated equipment has stopped.

When State is 1, there is ongoing communications with the associated equipment.

When State is 2, the driver is offline for this specific equipment. The driver has attempted to communicate with the associated equipment but has timed out for the final time.

Schneider Electric Egypt and North East Africa

Attachment(s)
sys1.jpg [134.25 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: