{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Where can I check the Input Output Map on the ATV320 drive?
Issue:
Checking Status of Digital Inputs on ATV320 drives

Product line:
Altivar 320, ATV320

Environment:
All models in range

Cause:
Troubleshooting and testing

Resolution:
The ATV320 has the ability to check the status of the Logic or Digital inputs.

On the default display navigate to NON > ION > LIA > LISI.
On this screen you will see the logic input state and be able to determine if the inputs are opening and closing as needed.

Schneider Electric Egypt and North East Africa

Attachment(s)
ATV320 LISI.JPG.jpg [41.69 KB]