{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Samsung Lithium Ion Battery; alarm status-LED indication


Issue:
Samsung Lithium Ion Battery; alarm status-LED indication

Product line:
Samsung Lithium Ion Battery

Environment:
All models, all serial numbers


Cause:
When the operating limits of the LIB system are exceeded, the system will protect itself from failure. System has been programmed with conditions and setpoints (e.g., over voltage, over temp) that create an Alarm or Fault state.
System provides indications and information about its health and operational status via LEDs on the BMS.

Resolution:
See chart below of alarm LEDs:

Image1 Image2 Image3 Image4

Resetting the System:
Reset system after release conditions are met by pressing and holding RESET button for 3-to-5 seconds on the SMPS assigned as System BMS.

If you cannot reset the alarm condition or require further support please call Schneider Electric Technical Support 877-537-0607

Schneider Electric Egypt and North East Africa