Search FAQs
How to connect to the Masterpact MTZ via NFC [Video]
Question:
How to connect to the Masterpact MTZ via NFC
Product String Reference:
Objective:
The objective of this video is to provide guidance of how to communicate with a Masterpact MTZ via NFC.
Product Line:
High Current Air Circuit Breakers
Environment:
N/A
Resolution:
How to connect to the Masterpact MTZ via NFC
Product String Reference:
- Top Level > Product Category > Buildings & IT > Partner Project Transactional > Air Circuit Breakers > ACB MTZ Communication
- Top Level > PR_Product_OPS_Structure > Circuit Breakers and Switches > High Current Air Circuit Breakers > Masterpact MTZ
Objective:
The objective of this video is to provide guidance of how to communicate with a Masterpact MTZ via NFC.
Product Line:
High Current Air Circuit Breakers
Environment:
N/A
Resolution:
- Download the Masterpact MTZ from the Play Store or App Store. Register if required. NFC will work both in circuit open and closed conditions. Micrologic X can communicate with internal battery and does not require power.
- Open the app and click NFC
- Hold it before the Micrologic X unit.
- When connected, it will be able to read the data from the Micrologic X
- Information provided include: Serial number, product reference, hardware and firmware reference.
Released for:Schneider Electric Egypt and North East Africa
Explore more
Range:
Explore more
Range: